We need your support
1. To select the part from the list.
2. If there are any other efficient/mathing part that I have missed
Requirement : We need two Buck Converters with Inverted output
Requirement Spec
Requirement 1 |
Buck & Negative Output Module / Inverting Converters |
Requirement Specs |
|
Voltage Source |
Battery |
Vin |
+12V |
Vout |
(-) 3V or (-)5V |
Iout |
Min :100 mA Typ : 300 mA
|
Application Details |
|
Requirement 2 |
Same as requirement 1 EXCEPT Vin is in the range of 3.3V to 5V |
We went through Power Management parts and shortlisted these parts :
Part # | Mnfr | Category | Iout (Max) | Vin (min - Max) | Vout (Min - Max) | # Pins | Package | Approx Price |
PTNN78000A | TI | Buck/Boost & Negative Output Module | 1.5 | 7 - 29 | -15 to -3 | 5 | S M / T T | $8.25 |
TPS63700 | TI | Inverting Converters | 1 | 2.7 - 5.5 | -15 to -2 | SON | $0.90 | |
TL497A | TI | Inverting Converters | 0.5 | 4.5 - 12 | -25 to 30 | DIP/SOIC | $0.86 | |
LT1054 | TI | Buck/Boost Charge Pump | 0.1 | 3.5 - 15 | -5 | DIP/SOIC | $1.00 |
I have another question :
While discussing on op-amp forum for part # OPA547, MC 33063 is recommended.
My query regarding this part is :
I am seeing of questions on forum pertaining to issues like part getting heated, drop in output voltage. So need your suggestion to use this part.
Also I want to understand this calcuation :
Vin - Vout(Vin + |Vout|) should be less than 40 V |
The other Vout that is provided between the lines, what does it mean?
Refering Fig 10 in the data sheet, how to calcuate the source current, (data sheet provided current for -12V output)
On referring different figures on schematic, Vin is quite confusing. For this configuraton (Inverting Output) what is the range of Vin (Min to Max)
General Question :
I cam across two categories
1. Buck converters with positive output, but can also be used for negative output by refering application diagrams provided in the data sheet
2. Inverting converters that are designed for negative output.
What is the difference between these two categories and which category is recommended?