I need to drive a full bridge MOSFET module at 100KHz. Generally, every other manufacturers provide the maximum switch voltage that the device can have in a Gate driver like 600V and 1200V which are common the gate drivers specs. The switch stress is 700V and 12A RMS current in my case. I m not able to find a good dual channel 1200V gate driver anywhere. Can i use this UCC27524A-Q1 driver. I need isolation as well. Does this driver provide isolation. If not, is there any TI mosfet driver that provides isolation. This is my first converter design. Pls someone help me.