This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2998 shutdown current

There are some additional questions.

Please tell me the total shutdown current max value.

Question

What uA is the maximum of I_SD at the time AVIN=3.3V?

What kohm is the maximum of Z_VDDQ?

What uA is the maximum of IQ_SD at the time "AVIN=3.3V PVIN=VDDQ=1.5V"?