This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409 minimum switching frequency

Other Parts Discussed in Thread: LM3409

Hi

COuld you explian why LM3409 has the minimum switching frequency 50kHz?  Thanks.

  • Hello Yun,

    I think the 50kHz is a recommend minimum switching frequency that is selected based on the tradeoffs between efficiency (better at low frequency) and solution size/cost (smaller at high frequency). Just like the maximum switching frequency can be programed to 5MHz. However frequency higher than 1MHz may be difficult to obtain due to gate driver limitation, high input voltage ad thermal considerations.

    You may refer to the LM3409 data sheet to calculate the toff and switching frequency base on customer’s application.

    Regards,

    Victor