Hi.
I am planning to use "LM3671" to supply "1.2V / 600 mA max power" on my product.
I will evaluate LM3671 with "AN-1395 LM3671 Evaluation Board".
I guess I need to place R1, R2, C1, C2 to configure the right output voltage of 1.2V.
By the way, it is not clear to me if L (2.2 uH), Cin (4.7 uF), Cout (10 uF) are already placed on the evaluation board according to the User's guide (AN-1395).
Are these components already there? Or do I need to order these parts separately?
Thank you in advance.