Hello,
Our customer use bq24650 by below conditions.
Vin: 18V, Vout:13V, Iout:10A
They use below FET.
In this case, switching FET becomes high temperature.
Thus, they would like to change to the Low Rds FET.
Please let me know the below question.
(1) reccomend FET
In the datasheet P.17 table 1, there are reccomend device for 10A output.
Are there any reccomend FET of TI ?
(2) maximum value of Qg/Ciss
Please let me know the maximum value of Qg and Ciss which can be driven by bq24650.
Ryuji Asaka