Hi,
in a new design i use the BQ24073 power manager to supply a 3.3 V LDO (TPS77633D) and when the battery is disconnected a load of 60 mA is enough to put in c.c. the output of the LDO. The power good pin of LDO lows to 0 but the power good of BQ24073 remains high. When the Li-Ion battery is connected to the TPS77633D the circuit seems working good.
Thanks for your help.