Hello,
I can use UCC28710 for below Isolated DCDC ?
Vin:8V - 16V
Vout: 24V
Iout : 3A
Best Regards,
Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Asaka,
UCC28710 is suitable for the AC input or or DC input application.
For your application, you may try some half bridge or push pull controllers.
Regards