I am looking to charge a 12V 26Ah VRLA battery with a max charge current of about 3.5 Amps and max input voltage of 16V.
From looking at the data sheet, it appears that the diagrams shown are for charging 6V batteries, so I was wondering what are the significant(if any) changes that need to be made in order to charge my battery?
I have already tried building the circuit the datasheet suggest, but I ran into errors with the pass transistor. I was using a PNP power transistor(2N5876), but I found that the DRVC pin doesn't supply a high enough voltage to put the pass transistor into the saturation mode.(ie Veb maxed at 5V for the transistor, but I have 16-2 = 14V that is required.
Is there a way to design around this restriction?