TPS54331 is used as 24V to 5V conversion.
The motor is connected to same 24V line.
Therefore,glitch is added from the motor.
Is it a problem although Glitch is about 13ns(50V)?
(It is not necessarily guarantee.)
Best regards,
Noda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I don't have any data for that, but 50 V is well above teh absolute maximum even for a short time like 13 nsec. I would recommend clamping teh input voltage to below the absolute maximum TPS54331 voltage. You could consider using TPS54360 (60 V max) as an alternative.