Hi
I have questions about the BQ20Z45 operation.
I had summarized below.
I want to receive detailed answers.
Please send me as soon as possible.
- Below -
1. If the PFIN bit of 'PF Status-SCANNING' is input(setting) in GUI, the PF bit of SAFETY STATUS is input (setting) is whether or not?
2. Since IT Enable, Disable of IT is possible? If possible, what is the way?
3. When UVP, there a way to clear 0% capacity?
4. Let me know how to set EDV including alarms function
5. After a full charge, CHG FET OFF is whether or not ?
6. What is the action of 'High Discharge Start Temperature' on the 1st Safety of DF in GUI ?
Thanks,
MS