Hey there,
I've studied the datasheet and eval board schematic but I'm still nto sure where I should connect my application circuit's VCC line. I am making a battery-powered consumer product using a single LiPo cell. Using the BQ24195 I want to charge the battery when it's dead via USB, then boost the battery output to 4.2 - 5.0v as a constant power supply when the application circuit is activated .
PMID seems to be the output point when used as a power bank, so I think this is where I should connect the VCC of my application. But SYS is considered the "system" voltage rail.
Which do I use?