This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54232 heat design

Other Parts Discussed in Thread: TPS54232

Hello,All

Let me ask you a question about heat design of TPS54232.

Recommended PCB LAYOUT is written on datasheet_P17 ,however do you have any formula between heat and GND dimension ?

I am looking forward to your reply.

Best regards.

  • The EVM for TPS54232 is built on a 2" x 2", 2 layer pcb.  The bottom layer is a dedicated ground plane with one smal signal etch.  The top layer is about 50% ground.  It is a conservative design to allow a low temperature rise to the IC junction.  In general, dc/dc converter ICs with integrated FETs use an exposed pad to transfer heat directly to an internal or bottom side ground plane that will usually be a full layer.  TPS54232 does not have an exposed thermal pad.  Te vias directly under the IC may help to transfer heat.  I do not have any calculations to determine required copper area.  I based that design on previous experience.  There is a plan to develop a PCB copper area calculator.  I do not know the time frame for it though.  Probably not soon enough to help with any current projects.   

  • Hi,Mr. John

    Thank you for reply.

    Best regards.

    Taichi.