Need circuit for 10-12 VDC isolated power at 1 amp from 12 vdc 20 amp power supply. Does anyone have a circuit diagram and recommended chip and parts?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sid,
If you refer to the TI Powerlab reference design section
http://www.ti.com/lsds/ti/analog/powermanagement/reference_design.page
and input the design parameters, you will get a list of posssible designs.For example the LM5022 is used on the PMP7899 reference design. This is a 48V output but it can be modified for a 12V output