This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS71818

 

Hi,
 
I have designed a board with a TPS71818-33 (DRV package) (in respect of datasheet). The board is powered by a 4.2V battery. OUT1 is always on.
 
I have got the following problem: when I switch on OUT2, OUT2 = 3.3V so it's OK but when I want switch off  OUT2,  OUT2 = 2.4V and the current raises up to 70mA ( When OUT 2 is on, the current is only 10mA).
 
I don't know what is the cause of this problem but I have an idea: when I have designed the board, I forgot the thermal pad in the footprint. On the datasheet, I saw  the thermal pad is connected to GND. On my board, the 4.2V track goes under the thermal pad. My board is varnished so I think my problem comes from this.


 
Before redesigning the board, I need to know if my problem comes from the thermal pad.
Thank you for your reply,
Regards,

Bailon Alexandre