This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2951 minimum ESR

In the data sheet it says:

Features section in front says >12 mohm
Next to last line on Page 15 says 20-30 mohm
Last line on Page 15, says to see Typical Chracteristics for specific ESR requirements - cannot find anything
What is the min ESR?
Also, on Page 15 it says that output capacitor should have a resonant frequency "less than" 500 kHz.  Is this correct?
  • No accounting for the data sheet.  The minimum esr is determined by the minimum phase margin for stability.  But the minimum phase margin is determined arbitrarily to be between 30 - 45degrees in accord with how conservative is the engineer writing the data sheet.  It would be best to use the higher minimum esr values in your design - to account for temperature variables.   Regarding the "resonant frequency", the data sheet should read "greater than" 500kHz - you do not want the resonant frequency of the capacitor anywhere near to the control loop bandwidth of the regulator.