I need a circuit or device to do the following:
Automotive application. 24V Truck supply. So it could be up to 28V. Output of 13.8V @ 10A.
Can be module or controller circuit. I have looked at the LM3150. Any other devices?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need a circuit or device to do the following:
Automotive application. 24V Truck supply. So it could be up to 28V. Output of 13.8V @ 10A.
Can be module or controller circuit. I have looked at the LM3150. Any other devices?
Thanks
A quick search shows TPS40170-Q1 is automotive qualified solution. You could also look at LM25088, LM5088, LM25117, LM25119.