This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27741-G1 change value for OCD

Other Parts Discussed in Thread: BQ27741-G1, BQ27742-G1

Dear all,

we use the bq27741-G1 for a single cell apllication. At the moment we use a 5mOhm shunt and the overcurrent cutoff is at 6,4A like the 34,2 mV OCD from default configuration indicate.

We can change the shunt to change the cuttoff for a lower overcurrent, but if we want a cuttoff in a higher range, there is no possibility to change the OCD-Value. In the Datasheet and Userguide is no documentation if you can change this value. Also there is no range in the Datasheet defined, so we think it must be changeable. Can you provide a documentation or a hint where we can find this! Thank you for your assistance.

Kind regards

   Max