Hello,
I am evaluating TPS65217C for an AM3352 based design. It utilizes AC and BAT supply inputs. During testing I have seen instances where AC input is connected but the unit either keeps running off of battery or goes into OFF state. ACPWR bit in the STATUS register (0x0A) is set in this state. The only way to recover it to start running off of AC and charge the battery is to cycle the AC input. My design is supposed to run off of AC most of the time and switch to BAT if AC fails. The system is unattended and I can't afford to have AC input go into this state.
From what I have seen the conditions that would put the PMIC into this state include:
* Slow AC ramp up (Function of the external power supply)
* Inrush current while trying to switch from BAT to AC
Is there a tested solution that would make the TPS65217C robust against AC input fluctuations?
Thanks,
Samir