Dear all,
I try to avoid having a separate powersupply just to wake up the bq20z45-R1 in a none host application when the battery is deeply discharged (like the application note SLUA608). Is there any way I can have the current register set to charge current 64 or 128 mA before Power on Reset (POR) just to get a small charging current increasing the battery voltage enough to get the gas gauge module awake taking over the control ?
Best regards
Kjell