So after running an initial lot of a battery with bq34z100 fuel gauge I have one piece that is displaying some weirdness, I have 0V on pin 2 Ven, checking dataflash its showing a battlow, and measuring 1.8V instead of the expected 7.4 (2S lion). all the dataflash and configuration looks identical to a good pack, what else could cause Ven to go low? or is there something else going on here?