As we are trying to design a product which can work properly around the world, SMPS has been adopted which allows various working frequencies and voltages. However, SMPS brings much higher noises.
In our application, we need to measure current at pA precision. Therefore, DC noises are crucial to us. Could I have suggestions on designing 0.1mV pp dc sources from wall plugs directly?
Output voltage: +12V and -12V
Working current: +12V: 600mA, -12V: 300mA
Any suggestion will be highly appreciated.
Thanks a lot.
Regards
Richie