I am using the TPS65270 in my Senior Capstone project to provide 5V and 3.3V from a 12V supply. I am new to SMPS design and the synchronous buck converter. Using an equation I found in a SPMS training module online:
L = (Vin-Vout)(Vout/Vin)/(Fsw*Iripple)
Where
Vin = 12V
Vout = 3.3V
Fsw = 400kHz (set with a 680kOhm resistor)
Iripple = 10% (1A Iload) = 0.1A
I calculate a minimum inductor size of approximately L = 60uH. (I am assuming I can use the larger 3.3V output inductor for the 5V output as well to keep part count down)
This is significantly larger than the 4.7uH used in the TPS65270 reference design for the evaluation module (http://www.ti.com/lit/ug/slvu474b/slvu474b.pdf). The datasheet seems to be lacking any kind of range or method of selection for the inductor.
After a bit of research on the TI forums, I found nothing for the TPS65270, but posts for other DC/DC SPMS ICs suggested that the IC would not operate over a large range of inductor values and would be configured for something closer to the 4.7uH in the reference design. Which leaves me with the question: How do I size and spec an inductor for my application? If my 60uH calculation is correct, I have an 82uH Wurth 74435588200 selected. However, if a 4.7uH or similar sized inductor is needed, I will select one with similar specs to the Wurth 744311470 suggested in the reference design.
Any help would be greatly appreciated.
-Charlie