This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z110 optimization and Battery Low Alarm

Hello Tim,

I am trying to run the optimization cycle of a 12V/22Ah battery. I discharged the battery at 2.8A. I set the Cell BL Set Volt Threshold to 1700mV. During the discharge cycle, I have a Battery Low Alarm. Does it affect the optimization cycle? 

Thanks,

Andy

  • Andy,

    The BATLOW alarm should not be set during the full discharge cycle, but it may set near the end. It should not cause the optimization cycle to abort, but you may need to calibrate the voltage if it is set during the full discharge.

    Tom