Hi Buddies,
I have build a POE board very close to the schematics in the SLUA469. The only thing i changed is R14 to get a 3.5V output instead and R21 to change POE class. Normally the power is working just fine - but sometimes when i start-up the POE the transformer is making a high frequency noise and everything gets pretty hot so i guess the efficiency falls for some reason.
I use approximately 1.5W from the power supply, so maybe this is too little?
Maybe you have a hint with things to check ?
Thanks in advance.