Hello,
In my application I need large storage capacitor (2 x 4700uF) on output side of a regulator (LMR12010), for driving GSM module. On primary side I have also even larger storage with higher voltage (12V) as a reservoir for sending warning message in case if aux. power supply is lost.
I works fine but I noticed unwanted voltage ripple on output voltage (3.6V). This ripple (300mVp-p) has quite low frequnecy from 8 to 50Hz depending on load.
I tried adding " feed forward capacitor with a value between 470pf and 1000pf across the top feedback resistor (R1)" as recommended in a datasheet, I tried to add additional low ESR ceramic 10uF capacitor right on output but non of it helps. Not even ripple voltage frequency has changed.
Any idea what should I do to reduce this quite big ripple voltage?
Thanks in advance
Janez Humar