Hi, I'm trying to base a design for a client on the TPS54383/6 which actually requires about 5A current for a single voltage. This brings me to my question - Can I keep same voltages on both outputs on the TPS54383 and combine them to get a higher current output? Also Could you suggest a chip from the TI product portfolio for 12V DC @ 10A? This would be used to drive a brushless motor.
Thanks!