This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24617 & POWER CIRCUIT RESET

Other Parts Discussed in Thread: MSP430F2254, BQ24617

Hi.....
I am using BQ24617 for charging the 7.2v Li-Ion battery. The Charge enable pin of BQ24617 is controlled by MSP430F2254(it is used for battery charge controller). And higher end controller is used as a master controller

We have Bootstrap loader circuit for MSP430 to progrmme the MSP via master controller. 

The DC-DC converter is connected to the charger o/p of BQ24617.

Problem:

When MSP430 getting programmed through Bootstraloader  via Master controller, it require RESET pin of the MSP pulled low (10 ms) then High ( Proper RESET) . due to this reason  CE Pin (driven by MSP) of the BQ24617 pulled low and then high ( As MSP pulled CE high  in his firmware) .  Due to such reason the Q1 and Q2 ( as refer to

Figure 1. Typical System Schematic in datasheet of BQ24617) of BQ24617 getting resets and I observe the approx 30ms voltage deep on power line( as refer to fig 1 , line goes to System) hence the whole circuits power supply interrupted and  I dose not satisfy the actual results.

Is there any relation/Dependency  between CE pin and the ACDRV/ pin? 

Putting the Bulck capacitor on power line will be the solution for my circuit? i do not want to add bulk capacitor.

Please help me in this regards!