Hi
Can bq24160 hold the input register even if voltage descended?
Is the register default setting if VIN becomes under UVLO?
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Can bq24160 hold the input register even if voltage descended?
Is the register default setting if VIN becomes under UVLO?
Regards,
PAN-M
Hello Pan-M,
Are there particular register values that you are concerned about?
The only events that typically result in changes to the register values are when new values are written via I2C and if the watchdog/safety timer is used and allowed to time out.
In the case of the watchdog safety timer if the counter is not cleared regularly by I2C command the device will reset the register values to default. (Pg. 20 of the datasheet)
In the event of UVLO there should be no change to the programmed register values.
Thank you for answer.
There is no specific register about which our customer is concerned.
Our customer think they would like to keep the value of the register only set up by I2C at the turn off.
After all, VIN seems to should be more than UVLO.
I understood it.
Thanks and Regards,
PAN-M