This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76801 - Vout Accurancy

Hello,

Would you mind if we ask Out Accurancy on TPS76801?
 
The data sheet shows following about Out Accurancy;

Conditions: –40°C< TJ< +125°C, VO + 1 V< VIN < 10V, 10 mA< IO< 1A
OUT Accuracy : (0.98)VO<VO<(1.02)VO


<Question>
If we use TPS76801 on the condition which is small terms of use range as following,
how much value of OUT Accuracy you can except?

Conditions:0°C~65°C(TJ), VO+1V < VIN < VO+3V, 10mA < IO < 0.5A
OUT Accuracy : (???)VO<VO<(???)VO

If you have following characteristics, is it possbile to send us them?  
- temperature dependance,
- input current dependence properties,
- output voltage dependence properties

Finally, if these contents are unofficial, could you send these replies to my E-mail address durectly?

We need your help.

Kind regards,

Hirotaka Matsumoto