This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220 with ADS1299

Other Parts Discussed in Thread: ADS1299, TLV61220

Hello,

I'm currently developing a medical device using the ADS1299, as it needs both a 3.3V and a 5V sources I'm using the TLV61220 to boost the 3.3V to 5V, in principle it works fine and I had some issues when connecting the load, then it started working fine but only for a limited time.

The TLV61220 boosts fine for around a couple of hours and then it stops working, my initial FB voltage is a bit over 500mV and then it drops to around 300mV. Then it remains like this for a couple of days and starts working again.

Any recomendations? I want to use at least 3 ADS1299 chips for my application but I'm not sure if a single TLV61220 give enough power for all of them.

Thanks in advance and regards.