This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR22007 Toko Inductor

Other Parts Discussed in Thread: LMR22007

Hello,

I desing a Hardware and im using the LMR22007 Voltage Regulator.

There are 4 Inductors recommended in the data sheet:

Type

Inductance [μH]

Saturation Current [A]

Dimensions [L x B x H] [mm]

MANUFACTURER

D1286AS-H-2R2M

2.2 μH, ±20%

1.3

2 x 1.6 x 1.2

TOKO

XFL3012-222MEC

2.2 μH, ±20%

1.6

3 x 3 x 1.2

Coilcraft

VLS252012T-2R2M1R3

2.2 μH, ±20%

1.3

2.5 x 2 x 1.2

TDK

PSI25201B-2R2MS

2.2 μH, ±20%

1.3

2.5 x 2 x 1.2

Cyntec

Im looking for the smallest variant of Toko but i can't even find this type on the Toko homepage.

And I can't find it on the homepages of different distributors.

Can you give me some Information of this Inductor?

Greets Nico