Hi,
I'm developing an automotive application where as my specifications I need to operate from 10 to 30V (trucks) input voltages. I wonder that can I use the BQ24040 as a LiIon charger without any pre-regulator? As in the product matrix TI inidcates its running till 30V. However in the datsheet there is a note about somewhat 6V over voltage protection kicks in. So what's the truth here? :)
Anyway if it doesn't works is there a suitable charger IC from TI portfolio for 10...30V input voltage?
Thanks a lot!
Zoltan