Hi,
I have several questions regarding the SLVA319C report.
I have simulated Gt(s) equation (7) on page 7 and did not get the same plot as Figure 2. I added an additional pole modeled by a stray capacitance of 10pF and arrived at the same plot. Is that what TI did here?
I used the equation (8) as well as (9) and modeled GPW(s) and did not get the same plot as Figure 3. When I added a factor of 100 to SE equation (11) I arrived at the same plot. Is there a factor of 100 missing in SE? What are the A and F values used for the plot in equation (11)? I used A = 12290 equation (11) of the TPS61170 datasheet and F = 1Mhz for my simulation. 100 also is the DC gain for GPW(s).
Finally I'm hoping to use the IC to go from 14V to 24V @ 150mA. Following the application report I arrived at a inductance of 63uH. Is that too large. The datasheet recommends 10uH~22uH.
Thanks,
Ken