This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24074 ILIM pin connection if USB500 mode enabled?

Other Parts Discussed in Thread: BQ24074

Greetings. I am using a bq24074 to charge a 400mAh battery. I have the unit set to limit the input current to 500mA by pulling EN1 high and tying EN2 to ground. It is not clear from the datasheet what I should do on the ILIM pin, however. From the datasheet, it seems like ILIM is not utilized if the USB500 mode is selected, but the datasheet also states that leaving ILIM disconnected will disable all charging. So, if I am using the USB500 mode, what should I do with the ILIM pin? Please let me know ASAP.

Thanks,

Chris