Hi Sirs,.
besides the Vin higher, what`s the features of LMZ31506 than EN2360 please,
it`s cause of the EN2360 package is smaller than LMZ31506....
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirs,.
besides the Vin higher, what`s the features of LMZ31506 than EN2360 please,
it`s cause of the EN2360 package is smaller than LMZ31506....
Hi Philip,
Please refer the attached file for the comparison. Although EN23xx package looks smaller, the actual "solution size" (if including external components) is larger than LMZ31506. Moreover, the thermal performance, EMI, and features of LMZ31506 is also superior.
Thanks for your considerations,
Hung