This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700 hissing noise

Other Parts Discussed in Thread: UCC28700

i am working on UCC28700 based adapter solution for 9V/1A, moment board is powered up i am hearing hissing noise what will be problem can any one help here to solve the problem???

Regards,

Datta

  • Hi

    Can you add more detailed information to  help us to understand the problem better?

    I.e. can you specify:

    - input voltage whne the hissing noise happens, AC or DC input?

    - load current level when the hissing happens?

    - does the hissing happen at every voltage and load, or just some?

    - does the hissing happen as input voltgae is increaseds lowly from zero?

    - are the transformer cores properly glued or clipped? could the hissing noise be coming from the transformer?

    - if you look at the output voltage, does it show any signs or oscillation or instability?

    - can you give more details of the transformer size, transformer inductance, transformer turn ratio, current sense resistor value, out capacitance value, etc?

     

    Thanks,

    Bernard