This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2490 Von / Voff Thresholds

Other Parts Discussed in Thread: TPS2490

Any recommendation on a circuit to increase the Von / Voff thresholds on the TPS2490? 

For example, setting Von ~ 40V and Voff ~ 34V ?

Thanks,

-- Mike --

  • There is an app note SLUA337 found on the the TPS2490 product page. I'll attach it if I'm lucky.

    slua337a.pdf
  • With a somewhat lower accuracy, and some provisions in functionality, it is possible to add a resistor from the output to the EN pin (R1 & R2 per the page 1 schematic)  to add some additional hysteresis to the existing internal hysteresis. 

    Untested values might be something like R1 = 57.6K, R2=2K, Rfeedback=604K.

    If the input voltage is between the thresholds and the output is shorted, the 2490 will be disabled.  Also, this assumes that the output is pulled (fully) low when off.