Hello all
I have a small converter using the LMR14006Y that goes from 24V to 12V
Components are according to webbench, L1=27uH Cout 4.7uF Cin 2.2uF and the usual 100nF boot , plus the diode and the resistor divider to get FB voltage.
I can draw max of 42mA and then the converter "sit" to a Vout to provide the 42mA (eg 5V)
I wish to draw the nominal .6A at 12V (as from webbench), what should I check to reach the desired target ?
If I draw less than 40mA the Vout is 12v as desired...
Thanks