This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TWL6030, TWL6032 battery charger: full charge current not reached

Other Parts Discussed in Thread: TWL6032, TWL6030

Hello,

I have a omap4460/twl6032(no power path) based custom board with battery pack and I'm trying to charge the battery over USB. I'm using a wall charger, which supports  2A output current. I configured the PMIC to 1500 mA charge current, 4.2V battery voltage, no input current limit, anti-collapse loop is active. I'm observing current from wall charger with USB power monitor. Unfortunately, I see only about 500mA flowing towards the board.
After some research i founded out that the VUSB voltage drops bellow limit and the anticollapse loop limits the input current.  Setting this threshold to minimum (4.2V) lead to increase of current up to 710mA. If the charger stops, the VUSB voltage is above 5.1V again. 

Then I experimented with TI's Blaze (http://www.omappedia.org/wiki/OMAP4_Blaze), which has an omap4430/twl6030 processor board. Unfortunately I observed similar behavior:  maximum input current only 900mA instead of 1500mA (no current limit  set) and VBUS is dropped to 4.2V while charging.

I tried my wall charger with other devices and measured current above 1.2 A. 

The question:  is  it possible to push the maximum input current ( 1500mA) into the charger? Can anybody give me any advices what could be wrong with usb charger?


Thanks in advance,

Regards,

Eugen Wagner


I attached the register dump of twl6030 captured while charging.

OMAPCONF (rev 1.68 built Mi 6. Nov 12:38:20 CET 2013)

HW Platform:
  Blaze
  OMAP4430 ES2.2 GP Device (STANDARD performance (1.0GHz))
  TWL6030  ES2.1 (EPROM rev7.0)
  TWL6040  ES1.1

SW Build Details:
  Build:
    Version: full_blaze-userdebug 4.2.2 JDQ39 eng.amn.20131212.175822 test-keys
    Pastry: Jelly Bean
    Type: userdebug
    Date: Do 12. Dez 17:59:02 CET 2013

  Kernel:
    Version: 3.4.34-01482-ge9515a7-dirty
    Author: amn@ux1278
    Toolchain: gcc version 4.6.x-google 20120106 (prerelease) (GCC)
    Type: #2 SMP PREEMPT
    Date: Fri Dec 13 15:43:19 CET 2013

REGISTER DUMP FOR TWL6030
=========================================================
BUS=1 SLAVE ADDR=0x48
---------------------------------------------------------
       0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f 
0x00: 12 30 19 02 01 00 01 00 19 25 17 03 01 00 00 00 
0x10: 01 02 00 00 00 00 00 00 00 00 00 00 00 00 00 01 
0x20: c0 2b 03 0f 18 00 00 2a 00 0a e0 00 20 02 00 00 
0x30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x40: 01 05 55 00 2b 00 01 05 05 00 3c 00 01 05 05 00 
0x50: 3e 00 01 01 55 00 00 06 01 01 55 00 00 06 01 01 
0x60: 55 00 00 06 01 05 55 00 2b 00 00 00 00 00 00 00 
0x70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x80: 07 05 55 0c 01 01 55 14 01 01 00 09 01 01 00 03 
0x90: 01 05 05 09 01 05 05 09 01 01 00 09 01 01 00 0a 
0xa0: 01 05 05 18 01 01 00 09 00 00 00 00 00 01 05 05 
0xb0: 01 05 55 01 05 05 07 05 55 07 05 55 01 05 05 01 
0xc0: 05 05 07 0d 55 07 05 55 07 05 00 07 01 55 07 05 
0xd0: 55 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0xe0: 7f 00 00 00 07 10 6a 03 00 00 00 80 1a 7f 04 80 
0xf0: 55 65 11 00 ff 01 7f 00 00 00 01 00 00 00 00 00 
=========================================================

BUS=1 SLAVE ADDR=0x49
---------------------------------------------------------
       0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f 
0x00: 51 04 30 c0 05 05 15 15 06 00 00 00 00 00 00 10 
0x10: 00 00 00 00 01 01 00 00 00 00 00 00 00 00 00 00 
0x20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 6b 00 
0x30: 00 00 00 06 02 00 00 00 00 00 00 00 00 00 00 00 
0x40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x50: 00 00 00 00 00 00 00 39 00 01 00 18 00 00 00 d8 
0x60: 01 c5 01 5f 01 15 03 96 01 01 00 71 02 32 02 d2 
0x70: 02 aa 02 ed 01 1d 00 9f 01 00 00 00 00 00 00 00 
0x80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x90: 00 00 00 35 07 00 00 00 00 00 00 00 00 00 00 00 
0xa0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0xb0: 00 00 00 00 00 00 00 00 00 00 ff 7f 00 00 05 00 
0xc0: 00 33 04 00 6c f1 00 00 1e 00 7e 00 00 00 00 00 
0xd0: 00 00 00 c6 f7 8a c6 f7 8a 00 00 00 00 00 00 00 
0xe0: 04 10 20 85 00 02 00 01 00 20 01 08 23 0e 0f 35 
0xf0: 1e 04 11 00 ff 64 00 00 00 00 00 00 00 00 00 00 
=========================================================

BUS=1 SLAVE ADDR=0x4A
---------------------------------------------------------
       0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f 
0x00: 07 07 07 07 07 07 07 07 07 07 00 00 00 00 00 00 
0x10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x40: 00 00 00 00 00 00 00 00 01 01 01 01 01 01 01 01 
0x50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
0x80: 2a 20 00 00 00 00 00 02 00 00 00 00 00 00 00 00 
0x90: 01 23 0e 06 18 0f 96 43 24 aa 00 04 15 16 15 01 
0xa0: 18 24 11 11 02 03 04 03 04 03 04 03 03 03 65 5e 
0xb0: 01 86 5e 01 85 5e 03 84 5e 02 a5 56 02 a3 5e 02 
0xc0: 85 5e 02 08 04 00 00 00 00 00 00 03 03 7d 01 7f 
0xd0: 71 7f 01 75 6d 04 0c 7f 7b 0a 06 02 7b 07 04 07 
0xe0: 00 ff 00 00 00 30 30 30 30 30 30 30 30 30 30 30 
0xf0: 30 30 30 30 30 30 30 30 30 30 30 30 30 30 30 30 
=========================================================