This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910 VDD3 for USB_VBUS of AM3352

Guru 20090 points
Other Parts Discussed in Thread: AM3352
Hello,
 
Can we use VDD3 for USB_VBUS of AM3352 ?

VDD3 output range is from 4.65V to 5.25V and USB_VBUS minimum voltage is 4.75V.
Thus, VDD3 output voltage don't meet USB_VBUS requirement.
 
However, we use VDD3 for USB_VBUS of AM3352 and other slave devices. We don't connect USB connector.
Therefore , VDD3 output current is few.
I think that VDD3 output range is on the condition of 100mA output and full temperature.
If VDD3 current is low, VDD3 output meets USB_VBUS requirement.
Is my understanding correct ?
 
If there are any concern about VDD3 for USB_VBUS of AM3352 please let me know.
 
Best Regards,
Ryuji Asaka