Hi,
Would you mind if we ask TPS2592ZL and TPS2592AL?
<Question>
Fault response of TPS2592ZL and TPS2592AL are latch-off.
When the UV failure occurred, which will the fault response be Auto-Retry or Latch-off?
Kind regards,
Hirotaka Matsumoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Would you mind if we ask TPS2592ZL and TPS2592AL?
<Question>
Fault response of TPS2592ZL and TPS2592AL are latch-off.
When the UV failure occurred, which will the fault response be Auto-Retry or Latch-off?
Kind regards,
Hirotaka Matsumoto
Matsumoto-san,
When the input voltage reaches the falling UVLO voltage, the device is completely off. There is no internal mechanism that tries to turn the device back on.
The device will turn back on when VIN is above the rising UVLO voltage, EN is above its turn on voltage, and there are no faults.
Regards,
Darwin
Matsumota- san
Yes, the Fault response of TPS2592ZL and TPS2592AL are Latch-off.
The Under volatge failure will turn off the the devcice and Gate signal to the internal MOSFET will be removed.
The Auto- Rety or Latch is applicable to over curent or short circuit conditions.
Best Regards
Dinesh
Darwin San,
Thank you for your prompt reply.
We got your saying completely!
Kind regards,
Hirotaka Matsumoto