This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2841 Duty Cycle



We design a Buck converter for LM2841X. The input voltage is 16V ~32V, output voltage is 3V , load current is 0.15A. The schematic is the same as that of Webench, L is 120uH, C is 22uF*2, Cboot is 150nF. We probe duty cycle by voltage of SW pin. 

We found that the duty cycle of the circuit is not constant. Why? The Buck should be in continuous conduction mode for the working condition, and the duty cycle should be constant. And for higher input voltage,  it is more obvious.

The following is the captured oscillator image. 3652.duty.tif

  • This could be simple instability or noise.  Did Webench select the 120uH inductor ?

    That seems rather large ?  You could try a smaller L.

    Be sure to follow all the appropriate guidlines in the data sheet regarding layout and input bypass.

    FD

  • Yes, Webench select 120uH. For 32V input, Webench even select 150uH inductor.

    How to determine whether it is instable or noise?

    When the probe is connected to SW pin, the output ripple increase very much.

  • I would try a smaller inductor as a test.  If that does not clean up the

    duty cycle I would look at you layout.  You can send us your layout and we

    can take a look at it.

    FD

  • Yes, a smaller inductor can improve the problem. But why? The Operating values in Webench show that the higher input voltage, the larger phase margin (more stable).  For large inductor, the circuit is stable for low input voltage. But for higher input voltage, the duty cycle is not constant. This is not the same as results of Webench. Why?

    For this working condition, what is the recommended value for inductor?