Hello, in LMZ35003 datasheet and manual it is reported that this device needs some copper areas beneath it.
does the AGND copper area need to be left completely floating ? in the datasheet it's reported that this area will connect to PGND in a single point; is this connection provided internally (connecting both 8 and 9 pins to PGND) ?
So the vias recommended near pin 37 are only thermal ?
Also the area that connects the phase switch nodes (6,7,21,22,23,24,38,41) is to be left floating ?
Thank you