Other Parts Discussed in Thread: TPS65910
Hi All,
Would you mind if we ask TPS65910?
<Q1>
If LDO or SMPS of the device works the current limit function, do all of LDO and SMPS stop outputting?
Or does the output which works the current limit function only stop?
<Q2>
After working the current limit function, please tell us restoration procedure from the failure.
<Q3>
DC output voltage shows Vout 1.8V±3% on the datasheet.
This value( Vout 1.8V±3%) is including "DC lead regulation" and "DC line regulation", or not?
Kind regards,
Hirotaka Matsumoto