Hello
It has designed by TPS51367 now.
Please give me the data of an open short examination.
Since he would like to consider it as reference data, please give.
The open short examination was done.
Spec
input:12V
V5 pin:5V
output:1.24V 11A
It ignites, when Vin and V5 pin are short-circuited.
Emitting smoke
・VIN-SLEW pin short
・VIN-VSNS pin short
・VIN-REFIN2 pin short
Since ignition and emitting smoke become a fire, they need to be coped with.
A measure is not made with an in-company rule in resin.
Are there any other methods?
Thank you