This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910A3 VDD3 input

Hi,

i am not using the VDD3 boost SMPS of TPS65910A3A1. according to the schematic checklist of this IC it is clear that the SW3 can be left floating and VFB3 should be connected to ground. For the input (VCC3) it is given that it should be connected to VCCs. what is meant by VCCs here? should I connect it to VBAT supply of PMIC? 

Also does the additional components like inductor and capacitors even if not used?

Thanks & Regards,

Nikhil