I am thinking about using the LT1764 in a new product. I would like the shut down pin, when active, to open up the output but I am not sure what it does, I can't find it in the DS. I mostly need to know if current from the load will flow into the out pin when it is shut down, and how much. Maybe there is a LDO that has Ioff specified? I would need about a 0.5 Amp 3.3V output from a 5V input. -40 to +85 Temp.
Thanks Tom