This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40490 Duty Cycle

Hello,


On the website for the TPS40490 the maximum Vout is listed as 45V with a 60V maximum input. I don't see this specification in the datasheet for TPS40490. Can someone confirm that the TPS40490 can only output 45V max and if that is the case, what is the minimum input voltage needed to achieve 45V output?


Thank you