I have an application that needs 3.3V and 5V from 4 Alkaline AA batteries. From what I read the AA voltage will vary from 1.5V to 1.1V so I'll get 6V to 4.4V. I was thinking to use one TPS62162 to convert from 6V-4.4V to 3.3V and then one LMR62421 to convert the 3.3V to 5V. I didn't know about SEPIC converter.
Now I'm thinking to use LMR62421 as SEPIC so can convert the 6V-4.4V to 5V and then use a LDO for 5V, do you think it is ok?
How can use the webench design the test the SEPIC design? On the datasheet the SEPIC converter use the WSON package but it only have one more pin the AGND, can it be made with the TSSOP package?
Thank you